Technical FAQs

Ask a Question

What is the interupting rate of the GJL36015M03?

Magnetic only circuit breakers do not have an interrupting rating. They are UL Recognized components and comply with NECrequirements for providing motor circuit protection when installed as part of a UL listed combination controller having motor overload protection.

CTA-ID : 2024287
Was this helpful?
What can we do to improve the information ?