Technical FAQs

Ask a Question

I am installing an NXL361200G breaker in a NA1200AWK enclosure. On a three wire system, does the neutral CT on solid neutral assembly SN1200NACT need to be hooked up to the breaker or not?

You do not have to hook up the neutral CT`s for three wire loads. Leave the CT terminals on the breaker open.

CTA-ID : 2024281
Was this helpful?
What can we do to improve the information ?