Technical FAQs

Ask a Question

What are the dimensions of the 9001KY3 enclosure?

Issue:
What are the dimensions of the 9001KY3 enclosure?

Product Line:
30mm Control Stations

Environment:
9001K/SK 30mm Control Stations

Cause:
Dimensions are needed for application.                                                

Resolution:
3- 5/8 inches wide 7-1/2 inches high and 3-17/32 inches deep
 
Was this helpful?
What can we do to improve the information ?