Technical FAQs

Ask a Question

Does Square D/SE offer a 225A meter socket for use with a QO142L225G load center?

Product Features

Product Line:

No, Use a 200A meter socket. The meter socket is continuously rated at 100% and the load centers are 80% rated per the NEC. 225A x .8 = 180A.

CTA-ID : 2024277
Was this helpful?
What can we do to improve the information ?