Technical FAQs

Ask a Question

Is there a 24 V field installable undervoltage trip for a Powerpact MG or MJ circuit breaker?

Issue:  
Looking for 24 Vac/Vdc UVR for Powerpact MGL or MJL breaker.  

Product line:  
Molded case circuit breakers

Environment:  
Powerpact MG and MJ circuit breakers

Resolution:  
S33668 is the field installable 24/30 volt AC/DC undervoltage trip.
Was this helpful?
What can we do to improve the information ?