Technical FAQs

Ask a Question

Will two pole QO-GFI circuit breakers work without bringing a load neutral back to the breaker?<br /><br />

Yes , the breakers will still work just fine . The load neutral connection needs to be made if and only if there is a load neutral wire. The white pigtail of the breaker must still be connected to the panel neutral to power the GFI Electronics and the Push-to-Test circuit. This would be for a 240vac load on a 120/240 vac system.

CTA-ID : 2023995
Was this helpful?
What can we do to improve the information ?