Technical FAQs

Ask a Question

What is the largest 3 pole breaker that can go into a QON442MS400 load center?

Issue:
Can I get a three pole 150A breaker for a QON442MS400 load center?

Product Line:
QO Load Center

Environment:
In a QO 3 Phase Load Center

Resolution:
The largest three pole breaker for this load center is a 100A QO3100.

CTA-ID : 2024274
Was this helpful?
What can we do to improve the information ?