Technical FAQs

Ask a Question

What are the part numbers to install an NQOD42L225, NQOD42L225CU , NQOD442L225 or NQOD442L225CU interior in an MH44 box?<br /><br /><br />

The following parts will be required per panel:

(2) 80110-288-03 (9`` rail extensions)
(1) 80110-291-02 (9`` MLO deadfront extension)
(4) 21590-17081 (rail extension screws)
(2) 80025-067-01 (deadfront screws)

These parts replace the main breaker kit.

CTA-ID : 2024268
Was this helpful?
What can we do to improve the information ?