Technical FAQs

Ask a Question

What is a Class 9999 Type MLPF?

Obsolete noise filter for the Class 9065 Type SP__ Motor Logic Plus overload relay. This protection is now provided built into the Motor Logic Plus overload relays.


CTA-ID : 2024450
Was this helpful?
What can we do to improve the information ?