Technical FAQs

Ask a Question

What is the difference between the 9001KYAF1 and 9001KYAF100 control station?<br />

9001KYAF1 is single hole 30mm control station enclosure to be used as an enclosure component for field assembly of a control station. The 9001KYAF100 is same control station with assembled operators by Square D. Customer must furnish a 9001 Control Station Key Sheet with order. Key sheet can be obtained from Customer Service or local field office. Also can be found in the Push button catalog 9001CT0001.

CTA-ID : 2024253
Was this helpful?
What can we do to improve the information ?