Technical FAQs

Ask a Question

Does Schneider Electric offer Manual Transfer Equipment kits for the QO 3-phase load centers?

Issue:
Product design features

Product Line:
QO three phase load centers

Environment:
Manuel Transfer kits

Cause:
Application

Resolution:
NO, the manual transfer equipment kits are ONLY available for QO single phase load centers.
 
Was this helpful?
What can we do to improve the information ?