Technical FAQs

Ask a Question

In the XVBC21 base, is the white terminal cover supposed to come with two mounting screws?

No. There was a design change that eliminated these two screws. Now there is only one screw provided for the terminal strip itself. The white cover is held in place by the lens unit when it is attached to the base.

CTA-ID : 2024238
Was this helpful?
What can we do to improve the information ?