Technical FAQs

Ask a Question

What is the current rating of a ZB6 bulb?

ZB6YA006 6V, 60mA
ZB6YJ012 12V, 40mA
ZB6YB028 28V, 24mA
ZB6YG095 110/230V, 1.8mA



CTA-ID : 2024446
Was this helpful?
What can we do to improve the information ?