Technical FAQs

Ask a Question

What is the replacement for the Q22200P breaker?

Issue:
Repair Parts

Product Line:
Hitch-N-Post

Cause:
Maintenance

Resolution:
The replacement breaker is obsolete, no longer available with no replacement.
Q22200P was a special 200A 2P Q2 breaker built for HITCH-N-POST METER PEDESTALS units.
The complete unit was a HNP2200CB, which included the breaker, BUT this is Obsolete and No longer available.


CTA-ID : 2024440
Was this helpful?
What can we do to improve the information ?