Technical FAQs

Ask a Question

What is the dimensions for a 9001KR9 , 9001SKR, 9001KR9P and 9001SKR9P when the handle is extended?

Issue:
What is the dimensions for a 9001KR9 , 9001SKR, 9001KR9P and 9001SKR9P when the handle is extended?

Product Line:
Harmony Push Buttons

Environment:
Harmony 30mm

Cause:
Product Specifications

Resolution:
1 and 5/16 inches


CTA-ID : 2024438
Was this helpful?
What can we do to improve the information ?