Technical FAQs

Ask a Question

Will the Hubbellock Receptacle Switch allow you to insert or remove a plug from the switch when it is in the ``On`` position?<br />

The interlocking linkage between the receptacle and switch mechanism prevents insertion or removal of the plug while the switch is in the ``On`` position or insertion of any plug other than specified. The interlocking mechanism also prevents the switch from being turned ``On`` if a plug has not been fully inserted into the receptacle.

CTA-ID : 2024432
Was this helpful?
What can we do to improve the information ?