Technical FAQs

Ask a Question

What is the part number(s) for the 6 inch lower horizontal wireway cover for a Model 6 LVMCC?

80450-141-50 - 20`` W X 6`` H horizontal wireway cover assembly (includes mounting hardware)
80450-141-54 - 20`` W X 6`` H horizontal ventilated wireway cover assembly (includes mounting hardware), used w/ 2500A horizontal bus

80450-141-51 - 25`` W X 6`` H horizontal wireway cover assembly (includes mounting hardware)
80450-141-55 - 25`` W X 6`` H horizontal ventilated wireway cover assembly (includes mounting hardware), used w/ 2500A horizontal bus

80450-141-52 - 30`` W X 6`` H horizontal wireway cover assembly (includes mounting hardware)
80450-141-56 - 30`` W X 6`` H horizontal ventilated wireway cover assembly (includes mounting hardware), used w/ 2500A horizontal bus

80450-141-53 - 35`` W X 6`` H horizontal wireway cover assembly (includes mounting hardware)
80450-141-57 - 35`` W X 6`` H horizontal ventilated wireway cover assembly (includes mounting hardware), used w/ 2500A horizontal bus


CTA-ID : 2024231
Was this helpful?
What can we do to improve the information ?