Technical FAQs

Ask a Question

Is the ``M4`` (low pressure cut-out) available on the 9013GSG..... pressure switches?

No, it is not available on the 9013GSG.. pressure switches. Only available on the 9013FSG.. and the 9013FYG... pressure switches.


CTA-ID : 2023961
Was this helpful?
What can we do to improve the information ?