Technical FAQs

Ask a Question

Are the QO load centers suitable for use in a portable applications?

Yes they can be used. They must follow the code for portable units. They should also make sure it is a NEMA 3R unit.

CTA-ID : 2023952
Was this helpful?
What can we do to improve the information ?