Technical FAQs

Ask a Question

992330, 3 pole 30A Circuit Breaker Replacement

Issue:
What is the replacement for a circuit breaker, 992330 for an old style ML panelboard?

Product Line:
Square D obsolete ML panelboards sold and supported in the 1960's.

Environment:
Replacement branch circuit breakers/maintenance.

Cause:
Are branch breakers still available for the obsolete ML panelboards?

Resolution:
The ML breakers and their replacements are now obsolete with no replacement. Consider replacing the panelboard with a new, current I-Line panelboard.     

 

CTA-ID : 2024428

DUPLICATE OF FA176128
Was this helpful?
What can we do to improve the information ?