Technical FAQs

Ask a Question

XPSMCWIN - customer wants to know if he can purchase one software package and use it to program multiple XPSMC* modules. What is the User licensing agreement for this software? Must he have one software CD for each XPSMC* module he purchases or can he use copies?<br /><br />

With 1 XPSMCWIN software, you can configurate multiple XPSMC16X or XPSMX32X controllers. The software licence is not linked to the unit.

CTA-ID : 2024217
Was this helpful?
What can we do to improve the information ?