Technical FAQs

Ask a Question

What happens with an ATV58 if the frequency is more less than the 5% +/- 50 or 60 Hz?

It is not shown in any of the books but, the drives will trip on input phase loss fault (PHF) at about 10% +/- 50/60 Hz.

CTA-ID : 2024216
Was this helpful?
What can we do to improve the information ?