Technical FAQs

Ask a Question

What are the dimensions of the HOMC42UC load center cover?

Issue:
Product Design Features

Product Line:
Homeline Load Center

Environment:
Cover dimensions

Cause:
application

Resolution:

The overall dimensions of this cover is 40.57" H x 15.44" W. The cover will over hang the load center enclosure by approximately 5/8"(0.62") on all sides.


CTA-ID : 2024212
Was this helpful?
What can we do to improve the information ?