Technical FAQs

Ask a Question

What are the repair parts for an EZML314225D, Series M03 branch unit?

Issue:
Current design repair parts

Product Line:
EZ Metering Equipment

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:

Replacement Drip Hood 73298-366-01
Customer Cover (includes labels) - EZML314225C
Cover Screws - 4020513002K
Meter Socket Cover (cover for one meter position) - EZMCRC
Parts Kit (one position, meter socket line side through tenant breaker base) - EZML1225KIT
Circuit Breaker RB Cover (one position) - BCV
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329771501
Equipment Ground Bar Assembly - 7329897053 (this includes 4 lugs mounted on the mounting bracket) 
Equipment Ground Bar Assembly Mounting Screws - 2142217101 (2 required)
End Closing Cap Kit - EZMCAP (this can be used on both the Left and Right sides of ANY EZM device)
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP


 
Was this helpful?
What can we do to improve the information ?