Technical FAQs

Ask a Question

What are the 9070AP3 and 9070AP4 fuse blocks?<br />

The 9070AP3 and 9070AP4 are a single secondary fuse kit for use on Type K and Type E control power transformers. The AP3 kit is used with VA sizes 25 through 150, and the AP4 is used with VA sizes 200 through 750. Both kits utilized a glass type fuse (not supplied), up to 30 amps. It is only available as field installable.


CTA-ID : 2023940
Was this helpful?
What can we do to improve the information ?