Technical FAQs

Ask a Question

Are there hangars available for mounting the NEMA 1 wireway in a vertical position?

The horizontal hangers can be converted to mount the wireway vertically. The wireway must be supported at least every 15 feet when installed vertically.


CTA-ID : 2023939
Was this helpful?
What can we do to improve the information ?