Technical FAQs

Ask a Question

What are the physical dimensions of the RWTBG100 grommet material?

The grommet is 0.39`` by 0.52``. The roll is 100 feet long.


CTA-ID : 2023936
Was this helpful?
What can we do to improve the information ?