Technical FAQs

Ask a Question

What features are provided with circuit breaker suffix # 1544

This suffix will provide for 1A/1B auxiliary switch, low temperature grease, anti-fugus treatment and the 24VDC UVR.


CTA-ID : 2024208
Was this helpful?
What can we do to improve the information ?