Technical FAQs

Ask a Question

What is the part number for the screw that is used to secure the upper & lower horizontal wireway cover?

21427-17322 - screw (10-32 x 1) for upper & lower horizontal wireway cover. 4 screws are required for each 12 inch high upper wireway cover, and 2 are required for each 6 inch high lower wireway cover.


CTA-ID : 2006957
Was this helpful?
What can we do to improve the information ?