Technical FAQs

Ask a Question

What is the difference between a STR25DP and a STR25DE trip unit for the Compact CK breaker?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The difference is the adjustments for long time.  The STR25DP is adjustable from
0.8 to 1 times rating plug (Io) value.  The rating plug can be changed.  The STR25DE is adjustable from 0.4 to 1 times the sensor (In) value.  The sensor cannot be changed.


CTA-ID : 2023934
Was this helpful?
What can we do to improve the information ?