Technical FAQs

Ask a Question

We are using a GC200E Ground Fault Relay. What should be done with the test terminals on the sensor GT1327?

If you want to do a test through the sensor, apply 120V on those open terminals. Otherwise, leave open.


CTA-ID : 2023924
Was this helpful?
What can we do to improve the information ?