Technical FAQs

Ask a Question

Does a H361SS safety switch come with Copper Blades, copper jaws , fuse clips and lugs

Yes, except for the lugs. They are available as factory installed copper lugs with Form SLC @ $149.00 list adder , or field install, order CL0306F @ $46.30 list, which include load and line base lugs.


CTA-ID : 2024396
Was this helpful?
What can we do to improve the information ?