Technical FAQs

Ask a Question

What is Class 2510 Type FW8?

This is manual starter manufactured to Eastman Kodak specifications. It consist of the standard 2510FO2 switch in cast aluminum enclosure. It is basically a 2510FW2 except in 2510FR enclosure, gasketed cover, o-ring seal on shaft, NEMA 4 nameplate and colored glyptal applied to the internal operator.

CTA-ID : 2024386
Was this helpful?
What can we do to improve the information ?