Technical FAQs

Ask a Question

Does the ATV31 have a sleep mode?

Go to the SET menu and scroll down to parameter tLS (Low Speed Operating Time).
After operation at LSP for a defined period, a motor stop is requested automatically.  The motor restarts if the frequency reference is greater than LSP and if a run command is still preset.

Reviewed 7/2011

CTA-ID : 2023706
Was this helpful?
What can we do to improve the information ?