Technical FAQs

Ask a Question

Can Class T fuses be used with Altivar 31 drives? The manual only references Class CC or J.

The ATV31 units were tested with the Class J fuses however the 600V version of the Class T fuses have equivalent ratings. So can use the 600V Class T fuses but not the 300V Class T fuses.

CTA-ID : 2023687
Was this helpful?
What can we do to improve the information ?