Technical FAQs

Ask a Question

What is the difference between a PK15GTA AND PK15GTAL?

Issue:
Product Features

Product Line:
Load Center Accessory

Cause:
Clarifying feature differences

Resolution:
The PK15GTA is the same as PK15GTAL except the PK15GTAL has an extra lug that will accept a #1 - 4/0 wire.


CTA-ID : 2023910
Was this helpful?
What can we do to improve the information ?