Technical FAQs

Ask a Question

Why is a GFI breaker in the HOM24L70RB, the QO24L70F/S and QO24L70RB load centers limited to using #10 wire?

Issue:
Product Features

Product Line:
Homeline Load Centers

Environment:
Wire size

Cause:
Application

Resolution:
The GFI breaker is longer than standard breakers, so the load center limits the load wire to #10 because of limited wire bending space.


CTA-ID : 2023902
Was this helpful?
What can we do to improve the information ?