Technical FAQs

Ask a Question

What is the the operating temperature range for a FAL Frame Circuit Breaker?

With re-rating for ambients outside the 20 deg C to 40 deg. C range, the circuit breaker will operate between -10 degree C to 60 Degree C


CTA-ID : 2024383
Was this helpful?
What can we do to improve the information ?