Technical FAQs

Ask a Question

ATV58HC10N4XZU dimensions

Width = 14.6 in (370 mm)
Height = 25.2 in (640 mm)
Depth = 14.2 in (360 mm)
Weight = 108 lbs (49 kG)


CTA-ID : 2024367
Was this helpful?
What can we do to improve the information ?