Technical FAQs

Ask a Question

What is the current rating on the contacts on form Y78 on a 9007 C68T10Y78?<br /><br />

Current rating is the same as the standard contacts even though these are gold flashed. However, gold flash is for use on low currents, less than 100 ma. Use of this device at higher current levels will oxidize the gold and eliminate its effectiveness. The same is also true for high cycling rates which will pound the gold and destroy it.


CTA-ID : 2023944
Was this helpful?
What can we do to improve the information ?