Technical FAQs

Ask a Question

Can I connect a Model 6 LVMCC directly to a Model 5 LVMCC, or do I need a transition section?

Model 6 LVMCC`s will splice directly to a Model 5 LVMCC, provided the Model 5 was built after May 1992. If the Model 5 was built prior to May of 1992 a custom splice kit is required. When placing an order, provide the existing Model 5 LVMCC factory order number (found on the UL structure nameplate label).


CTA-ID : 2024182
Was this helpful?
What can we do to improve the information ?