Technical FAQs

Ask a Question

Can a Main Circuit Breaker Kit be field installed on a QON130L200I OEM Mounting Base?

Yes, this Main Lug OEM Mounting Base can be field converted to a Main Breaker OEM Mounting Base. A QOM2-VH Main Circuit Breaker Kit, 100 - 200 ampere (QOM2100VH - QOM2200VH), can be field installed to replace the factory installed main lugs. The final acceptance of this component is dependent upon its installation and use in complete equipment submitted to Underwriters Laboratories, Inc.


CTA-ID : 2024557
Was this helpful?
What can we do to improve the information ?