Technical FAQs

Ask a Question

Can a Main Circuit Breaker Kit be field installed on a QON11224L125I OEM Mounting Base?

Yes, this Main Lug OEM Mounting Base can be field converted to a Main Breaker OEM Mounting Base. A QOM-VH Main Circuit Breaker Kit, 50 - 125 ampere (QOM50VH - QOM125VH), can be field installed to replace the factory installed main lugs. The final acceptance of this component is dependent upon its installation and use in complete equipment submitted to Underwriters Laboratories, Inc.


CTA-ID : 2024548
Was this helpful?
What can we do to improve the information ?