Technical FAQs

Ask a Question

What is the temperature rating of the D10 disconnect switch lugs?

Dependent on switch in question; values as follows:

D10S1, D10S2, D10S1H & D10S2H = 60 Degrees Celsius
D10S3, D10S4, D10S3H & D10S4H = 60/75 Degrees Celsius


CTA-ID : 2024173
Was this helpful?
What can we do to improve the information ?