Technical FAQs

Ask a Question

Will a Square D 9007 lever arm work on the LS2YMB4N Honeywell limit switch?

No. Honeywell`s shaft size is 0.284`` and Square D`s shaft size is 0.44``. The form Y249 is .28`` diameter shaft on the 9007


CTA-ID : 2024547
Was this helpful?
What can we do to improve the information ?