Technical FAQs

Ask a Question

What style of pilot devices do we currently use on Model 6 LVMCC starter units ?

Model 6 LVMCC`s use XB5 (plastic) 22mm pilot devices as standard.  XB4 (metal) 22mm and 9001 Type K 30mm are optional pilot devices that are available.  Note that 9001 Type K 30mm pilot devices are not available on Compac 6 units (6`` starter units).  See the document link for pilot devices in the On-Line Digest.

CTA-ID : 2009216
Was this helpful?
What can we do to improve the information ?