Technical FAQs

Ask a Question

Do contacts come with a XD5PA12 ?

Yes. Contacts are included with the XD4/5 joysticks. They use a special contact and are not replaceable.


CTA-ID : 1359
Was this helpful?
What can we do to improve the information ?