Technical FAQs

Ask a Question

What is the part number for the 1/4 turn fastener used on Model 5 & 6 LVMCC doors?

Issue:
What is the part number for the 1/4 turn latch used on Model 5 & 6 LVMCC doors?

Product Line:
Model 5 and 6 motor control centers.

Environment:
Products sold in the United States.

Cause:
Maintenance.

Resolution:
The 1/4 turn fastener components consist of the 1/4 turn fastener and the 1/4 turn fastener retaining clip.  Note that a kit of 15 1/4 turn fasteners and retaining clips is also available.  

80420-654-01 - 1/4 Turn Fastener
80420-655-01 - 1/4 Turn Fastener Retaining Clip

80450-410-50 - Kit of 15 1/4 Turn Fasteners & Retaining Clips



CTA-ID : 2021382
Was this helpful?
What can we do to improve the information ?