Technical FAQs

Ask a Question

What is the control coil operating voltage range for the Class 8903 Type L or Type LX Lighting Contactor?<br />

85% to 110% of marked or rated voltage.



CTA-ID : 2024199
Was this helpful?
What can we do to improve the information ?