Technical FAQs

Ask a Question

Will the IP40 rating of the two head XB4 operators be upgraded to an IP66 just by virtue of adding the ZBW008 boot?

Yes, IP66 for booted push button heads


CTA-ID : 2024536
Was this helpful?
What can we do to improve the information ?